Metadata-Version: 2.1
Name: nanotec-nanolib-linux
Version: 0.8.0
Summary: Communication and controlling library for Nanotec motor controller.
Home-page: http://nanotec.com
Author: Nanotec Electronic GmbH & Co. KG
Author-email: support@nanotec.de
License: Creative Commons Attribution 3.0 Unported License. Creative Commons Attribution-NoDerivatives 4.0 International License.
Platform: UNKNOWN
Classifier: Development Status :: 3 - Alpha
Classifier: Environment :: Console
Classifier: Intended Audience :: Developers
Classifier: Natural Language :: English
Classifier: License :: Creative Commons Attribution 3.0 Unported License. Creative Commons Attribution-NoDerivatives 4.0 International License.
Classifier: Operating System :: POSIX :: Linux
Classifier: Programming Language :: C++
Classifier: Programming Language :: Python :: 3.7
Classifier: Programming Language :: Python :: Implementation :: CPython
Classifier: Programming Language :: Python :: Implementation :: PyPy
Classifier: Topic :: Scientific/Engineering
Classifier: Topic :: Scientific/Engineering :: Human Machine Interfaces
Classifier: Topic :: Software Development :: Libraries
Classifier: Topic :: System :: Hardware :: Hardware Drivers
Requires-Python: >=2.7, !=3.0.*, !=3.1.*, !=3.2.*, !=3.3.*, !=3.4.*
Description-Content-Type: text/markdown
License-File: LICENCE

# Nanolib
This is the Python Windows version of the Nanolib.

## Prerequisites Windows
1. A python 3 installation is required, we recommend the official version from [python.org](https://www.python.org/downloads/windows/).
2. We recommend using a virtual environment before installing nanoteclib, open a CMD and use the following commands to setup a virtual environment:
   ```cmd
   mkdir test_project
   cd test_project
   python -m venv .env
   .env\Scripts\activate.bat
   ```
   In case the setup was successful the CMD is prefixed with `(.env)`, e.g. `(.env) C:\test_project>`
3. The package 'wheel' is necessary to install nanoteclib:
   ```cmd
   pip install wheel
   ```

## Prerequisites Linux
1. A python 3 installation is required.
2. We highly recommend using pip and "virtual environment". Install both with the following bash command:
   ```bash
   sudo apt install python3-pip python3-venv -y
   ```
3. We recommend using a virtual environment before installing nanoteclib, use the following commands to setup a virtual environment:
   ```bash
   mkdir test_project
   cd test_project
   python3 -m venv .env
   source ./.env/bin/activate
   ```
   In case the setup was successful the bash is prefixed with `(.env)`, e.g. `(.env) username@hostname:~/test_project$ `
4. The package 'wheel' and 'setuptools' is necessary to install nanoteclib:
   ```bash
   pip3 install wheel
   pip3 install setuptools
   ```
5. The library requires access to the serial port. To grant access, add the User to the dialout group
   ```bash
   sudo adduser $USER dialout
   ```

## Installation
To install Nanolib use pip with the following bash script:
- Linux:
  ```bash
  pip3 install PATH_TO_NANOTEC_LIB_ZIP/nanoteclib-N.N.N.zip
  ```
- Windows
  ```cmd
  pip install PATH_TO_NANOTEC_LIB_ZIP/nanoteclib-N.N.N.zip
  ```

where `N` is the actual number of the nanoteclib.