Metadata-Version: 2.1
Name: nanotec_nanolib_linux_arm64
Version: 1.2.1
Summary: Communication and controlling library for Nanotec motor controller.
Home-page: http://nanotec.com
Author: Nanotec Electronic GmbH & Co. KG
Author-email: support@nanotec.de
License: Creative Commons Attribution 3.0 Unported License. Creative Commons Attribution-NoDerivatives 4.0 International License.
Description: # Nanolib
        This is the Python Windows version of the Nanolib.
        
        ## Prerequisites Windows
        1. A python 3.7+ installation is required, we recommend the official version from [python.org](https://www.python.org/downloads/windows/).
        2. We recommend using a virtual environment before installing nanoteclib, open a CMD and use the following commands to setup a virtual environment:
           ```cmd
           mkdir test_project
           cd test_project
           python -m venv .env
           .env\Scripts\activate.bat
           ```
           In case the setup was successful the CMD is prefixed with `(.env)`, e.g. `(.env) C:\test_project>`
        3. The package 'wheel' is necessary to install nanoteclib:
           ```cmd
           pip install wheel
           ```
        
        ## Prerequisites Linux
        1. A python 3.7+ installation is required.
        2. We highly recommend using pip and "virtual environment". Install both with the following bash command:
           ```bash
           sudo apt install python3-pip python3-venv -y
           ```
        3. We recommend using a virtual environment before installing nanoteclib, use the following commands to setup a virtual environment:
           ```bash
           mkdir test_project
           cd test_project
           python3 -m venv .env
           source ./.env/bin/activate
           ```
           In case the setup was successful the bash is prefixed with `(.env)`, e.g. `(.env) username@hostname:~/test_project$ `
        4. The package 'wheel' and 'setuptools' is necessary to install nanoteclib:
           ```bash
           pip3 install wheel
           pip3 install setuptools
           ```
        5. The library requires access to the serial port. To grant access, add the User to the dialout group
           ```bash
           sudo adduser $USER dialout
           ```
        
        ## Installation
        To install Nanolib use pip with the following bash script:
        - Linux:
          ```bash
          pip3 install PATH_TO_NANOTEC_LIB_ZIP/nanolib_python_linux_#.#.#.tar.gz
          ```
        - Windows
          ```cmd
          pip install PATH_TO_NANOTEC_LIB_ZIP/nanolib_python_win_#.#.#.zip
          ```
        
        where `N` is the actual number of the nanoteclib.
Platform: UNKNOWN
Classifier: Development Status :: 3 - Alpha
Classifier: Environment :: Console
Classifier: Intended Audience :: Developers
Classifier: Natural Language :: English
Classifier: License :: Creative Commons Attribution 3.0 Unported License. Creative Commons Attribution-NoDerivatives 4.0 International License.
Classifier: Operating System :: POSIX :: Linux
Classifier: Programming Language :: C++
Classifier: Programming Language :: Python :: 3.7
Classifier: Programming Language :: Python :: 3.8
Classifier: Programming Language :: Python :: 3.9
Classifier: Programming Language :: Python :: 3.10
Classifier: Programming Language :: Python :: 3.11
Classifier: Programming Language :: Python :: 3.12
Classifier: Programming Language :: Python :: Implementation :: CPython
Classifier: Programming Language :: Python :: Implementation :: PyPy
Classifier: Topic :: Scientific/Engineering
Classifier: Topic :: Scientific/Engineering :: Human Machine Interfaces
Classifier: Topic :: Software Development :: Libraries
Classifier: Topic :: System :: Hardware :: Hardware Drivers
Requires-Python: >=2.7, !=3.0.*, !=3.1.*, !=3.2.*, !=3.3.*, !=3.4.*
Description-Content-Type: text/markdown