Metadata-Version: 2.1
Name: nanotec-nanolib-win
Version: 1.3.1
Summary: Communication and controlling library for Nanotec motor controller.
Home-page: http://nanotec.com
Author: Nanotec Electronic GmbH & Co. KG
Author-email: support@nanotec.de
License: Creative Commons Attribution 3.0 Unported License. Creative Commons Attribution-NoDerivatives 4.0 International License.
Description: # Nanolib
        
        This is the Python version of NanoLib with an example application. <br>
        The NanoLib offers an easy to use library to control Nanotec devices.
        
        [www.nanotec.de](https://www.nanotec.de/)
        
        ## Example Application
        ### Overview and Structure
        The CLI example application provides a menu interface where the user can execute
        the different library functions. The menu offers the user the possibility to <br>
        easily and quickly select and execute all functions supported by NanoLib. <br>
        The menu entries are context based and will be enabled or disabled, depending on
        the state.<br>
        To enable all entries you have to:
        1. Scan for hardware buses
        2. Connect to a found harwdare bus
        3. Scan for devices on the opened hardware bus
        4. Successfully connect to a found device<br>
         
        With this example application it is possible to:<br> 
        - do a hardware bus scan
        - open a found bus hardware (several hardware buses allowed)
        - close an opened bus hardware
        - scan for devices on opened hardware bus(es)
        - connect to a found device (several devices allowed)
        - disconnect from a connected device 
        - read device informations
        - update the firmware
        - update the bootloader
        - upload a NanoJ program
        - run/stop a NanoJ program
        - reboot a device
        - set logging and logging callback parameters
        - auto tune a motor (may require manual steps before)
        - get a motor to rotate
        - use the object dicationary interface for reads/writes
        - sample data
        - scan for Profinet devices
        - etc.
        
        The application menu and the supported NanoLib functionality is logically structered into several files:<br>
        Files with \*_functions_example.py contain the implementations for the NanoLib interface functions.<br>
        Files with \*_callback_example.py contain implementations for the various callbacks (scan, data and logging).<br>
        Files with menu\_\*.py contain the menu logic and code.<br>
        Example.py is the main program, creating the menu and initializing all used parameters.<br>
        Sampler_example.py contains the example implementation for sampler usage.<br>
        
        ### Windows
        #### Prerequisites
        - A python 3.7 up to python 3.12 installation is required. We highly recommend the official version <br>
          from [python.org](https://www.python.org/downloads/windows/).<br>
        - We recommend using a virtual environment before installing NanoLib:
        1. Open a command prompt (e.g. powershell) and use the following commands to setup a virtual environment:
           ```cmd
           cd <nanolib_directoy>
           python3 -m venv .env
           .\.env\Scripts\Activate.ps1
           ```
           **_Note:_** Depending on the used Python version, the names and location of the activation script may differ.<br>
           In case the setup was successful the CMD is prefixed with `(.env)`.<br>
        2. The package 'wheel' is necessary to install NanoLib as egg:
           ```cmd
           pip3 install wheel
           ```
        - Install [HMS - Ixxat VCI 4 driver](https://hmsnetworks.blob.core.windows.net/nlw/docs/default-source/products/ixxat/monitored/pc-interface-cards/vci-v4-0-1240-windows-11-10.zip?sfvrsn=2d1dfdd7_69) and connect CAN adapter (optional).
        - Install [PEAK device driver and PCAN API](https://www.peak-system.com/quick/DrvSetup) and connect CAN adapter (optional).
        - Connect all devices to your adapter(s) according to the user manual and power on the devices.
        
        #### Installing the NanoLib Egg 
        To install the Nanolib egg open a command promt and change to the<br>
        directory where the nanolib_python_win_N.N.N.zip file is located and<br> 
        use the following command to install the Nanolib into your python (virtual) environment:
        ```cmd
        pip3 install nanolib_python_win_N.N.N.zip
         ```
        Wait for the console to produce a success report ending on "Successfully installed nanotec_nanolib_win_N.N.N".<br>
        **_Note:_** Where `N.N.N` is the actual version of the NanoLib. <br>
        - To check if the installation has worked open up a python shell by executing Python:
        ```cmd
        python3
        ```
        - Inside the python shell import the NanoLib and press Enter:
        ```python
        import nanotec_nanolib
        ```
        If no error shows, the installation was successful.<br>
        You can now leave Python by typing exit() and press Enter.<br>
        
        #### Running the example project
        To run the example application, unzip the downloaded nanolib_python_win_N.N.N.zip file, 
        open a command prompt and change to the extracted example directory (example/nanolibexample).
        Use the following command to start the application:
        ```cmd
        python3 example.py
        ```
        
        ### Linux
        #### Prerequisites
        - A python 3.7 up to python 3.12 installation is required. We highly recommend the official version <br>
          from [python.org](https://www.python.org/downloads/).<br>
        - We recommend using a virtual environment before installing NanoLib:
        1. Open a command prompt (e.g. powershell) and use the following commands to setup a virtual environment:
           ```bash
           cd <nanolib_directoy>
           python3 -m venv .env
           source .env/bin/activate
           ```
           **_Note:_** Depending on the used Python version, the names and location of the activation script may differ.<br>
           In case the setup was successful the CMD is prefixed with `(.env)`.<br>
        2. The package 'wheel' is necessary to install NanoLib as egg:
           ```bash
           pip3 install wheel
           ```
        - Install [HMS Ixxat ECI driver](https://hmsnetworks.blob.core.windows.net/nlw/docs/default-source/products/ixxat/monitored/pc-interface-cards/eci-linux.zip?sfvrsn=19eb48d7_53) and connect CAN adapter (optional).
        - Download, build and install [PEAK device driver for linux and PCAN API](https://www.peak-system.com/quick/PCAN-Linux-Driver) and connect CAN adapter (optional).
        - Connect all devices to your adapter(s) according to the user manual and power on the devices.
        
        #### Installing the NanoLib Egg 
        To install the Nanolib egg open a command promt and change to the<br>
        directory where the nanolib_python_linux_[arm64_]N.N.N.tar.gz file is located and<br> 
        use the following command to install the Nanolib into your python (virtual) environment:
        ```bash
        pip3 install nanolib_python_linux_[arm64_]N.N.N.tar.gz
         ```
        Wait for the console to produce a success report ending on "Successfully installed nanotec_nanolib_linux_[arm64_]N.N.N".<br>
        **_Note:_** Where `N.N.N` is the actual version of the NanoLib. <br>
        - To check if the installation has worked open up a python shell by executing Python:
        ```bash
        python3
        ```
        - Inside the python shell import the NanoLib and press Enter:
        ```python
        import nanotec_nanolib
        ```
        If no error shows, the installation was successful.<br>
        You can now leave Python by typing exit() and press Enter.<br>
        
        #### Running the example project
        To run the example application, open a command prompt, untar and unzip the downloaded <br>
        nanolib_python_linux_[arm64_]N.N.N.tar.gz file and change to the extracted example <br>
        directory (example/nanolibexample). Use the following command to start the example application:
        ```bash
        python3 example.py
        ```
Platform: UNKNOWN
Classifier: Development Status :: 3 - Alpha
Classifier: Environment :: Console
Classifier: Intended Audience :: Developers
Classifier: Natural Language :: English
Classifier: License :: Creative Commons Attribution 3.0 Unported License. Creative Commons Attribution-NoDerivatives 4.0 International License.
Classifier: Operating System :: Microsoft :: Windows :: Windows 10
Classifier: Programming Language :: C++
Classifier: Programming Language :: Python :: 3.7
Classifier: Programming Language :: Python :: 3.8
Classifier: Programming Language :: Python :: 3.9
Classifier: Programming Language :: Python :: 3.10
Classifier: Programming Language :: Python :: 3.11
Classifier: Programming Language :: Python :: 3.12
Classifier: Programming Language :: Python :: Implementation :: CPython
Classifier: Programming Language :: Python :: Implementation :: PyPy
Classifier: Topic :: Scientific/Engineering
Classifier: Topic :: Scientific/Engineering :: Human Machine Interfaces
Classifier: Topic :: Software Development :: Libraries
Classifier: Topic :: System :: Hardware :: Hardware Drivers
Requires-Python: >=2.7, !=3.0.*, !=3.1.*, !=3.2.*, !=3.3.*, !=3.4.*
Description-Content-Type: text/markdown